RealSense Support

Can someone help me on how to get rs-convert.exe?

Comments

15 comments

  • MartyG

    Hi Vyas K  If you are using Windows and have installed the 793 mb RealSense SDK software from the Releases page, you can find an executable exe of rs-convert in the SDK's Tools folder.  You can locate this easily by right-clicking on the RealSense Viewer program launch icon the SDK installer will have placed on the Windows desktop and selecting the Open file location menu option.

    rs-convert should be launched from the Windows Command Prompt text interface instead of with a double left click in the folder.  You can find the Command Prompt by typing command into the search box at the bottom of the Windows screen, next to the corner button where the computer is shut down.

    0
    Comment actions Permalink
  • Vyas K

    I tried running the executable but it doesn't seem to doanything. When I try typing rs-convert.exe in cmd, it says not found. i have installed sdk and also recorded a bag file in it which I want to get ply frames out of

     

    0
    Comment actions Permalink
  • MartyG

    The rs-convert command on its own will not perform a conversion.  You need to specify in the launch command the type of conversion that you want to perform (e.g extract the bag to log format), the filename of the bag, etc.  A list of conversion commands and an example command are at the rs-convert web-page:

    https://github.com/IntelRealSense/librealsense/tree/master/tools/convert 

    Also, rs-convert exe should be launched in the Command Prompt from the SDK's Tools folder.  An easy way to go to that folder in Command Prompt is:

    1.  Go to the Tools folder on the Windows desktop using the previously mentioned shortcut.

    2.  In the address bar at the top of the folder window, left-click on the end of the address text-box to convert it to the Windows-format address C://Program Files (x86)/Intel RealSense SDK 2.0/Tools

    3.  Copy the contents of the address box with CTRL-C and go to the Command Prompt window.

    4.  Type cd followed by a space and use CTRL-V to paste the address into the Command Prompt window and press return.  The directory will change to the Tools folder.

    5.  Input the rs-convert conversion command.

     

     

    1
    Comment actions Permalink
  • Vyas K

    I got it to run. So the video I haev taken was at 15fps in depth. is there a way I can manipulate how many frames I get per second and also the names of the frames that gets written in the folder?

     

    0
    Comment actions Permalink
  • MartyG

    I am not aware of a way to manipulate FPS with rs-convert.  In regards to file naming though, whatever custom file name that you specify in the path that you provide in your rs-convert launch instruction should be used by rs-convert.

    https://github.com/IntelRealSense/librealsense/issues/7033#issuecomment-669215540 

    0
    Comment actions Permalink
  • Waseemshariff126

    Hi, 

    I recently bought a new Intel L515 LiDar camera. I am trying to convert the recorded BAG files to PNG, but I see there's no "rs-convert.exe" in SDK's Tools folder. On the GitHub page, all I could find are the CPP files but there isn't any exe file. May be I am doing it wrong. Please let me know. Thanks in advance. 

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Waseemshariff126  If you are using Windows then rs-convert.exe should be in the Tools folder.  This folder can be found by right-clicking on the RealSense Viewer launch shortcut icon that is placed on the Windows desktop and selecting the 'Open file location' menu option once the full RealSense SDK has been installed by the automated installer file in the 'Assets' file list on the SDK Releases page.  The rs-convert.exe file should still be present in the folder even if you have an L515.

    https://github.com/IntelRealSense/librealsense/releases

     

     

     

    If you installed the RealSense SDK on Linux then the pre-built executable versions of the sample programs should be in the /usr/local/bin folder.  If the SDK was built from source code with CMake in Linux then the examples are built by including the term DBUILD_EXAMPLES=true in the CMake build instruction.

    An example of an L515 owner successfully using rs-convert with it on Windows is at the link below.

    https://github.com/IntelRealSense/librealsense/issues/9288

    1
    Comment actions Permalink
  • Waseemshariff126

    Thank you so much for your quick response. It worked fine. 

    0
    Comment actions Permalink
  • MartyX Grover

    You are very welcome.  That's great to hear that it is working for you.  Thanks very much for the update! 

    0
    Comment actions Permalink
  • Waseemshariff126

    Hi,

    I explored the working of L515. I set the resolution to 640x480 with 30 FPS for all cameras: Depth, Infrared, and RGB. But while converting the BAG files to PNGs, I observed that the number of processed frames are varying. Can you please help us with this? 

    The below example data was recorded for 10 minutes and a few seconds. 

    I was assuming that the RGB camera was taking a long time to stop recording, which may explain the additional frames. That, however, is not the case. Throughout the time frame, these frames are produced.

    I also tried the Depth quality tools to modify settings, but it didn't help.

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Waseemshariff126  It would not be my expectation that depth / infrared and RGB color frame counts would match precisely, as the RGB image is produced by a separate sensor component in the camera, whilst depth / infrared comes from the same sensor.  A RealSense team member in the link below explains how there can be a time offset between depth and RGB.

    https://github.com/IntelRealSense/librealsense/issues/1548#issuecomment-389070550

    The closeness of your depth / infrared and color frame counts is actually one of the best that I have seen.

    The rs-convert tool auto-names files according to frame timestamp, so comparing timestamps would be the best way to find out which frames of different types correspond to each other at a given instant in time.

    Further discussions about how depth and RGB sensors sync temporally (not to be confused with multiple-camera 'hardware sync') can be found here:

    https://github.com/IntelRealSense/librealsense/issues/8726#issuecomment-812556071

    0
    Comment actions Permalink
  • Sohampadhye1998

    Hello MartyG

    I'm getting only one frame from .bag file and few frames data 

    Please help to get each frame and each reading during entire span.

    I want the readings along with the frame number so that I can synchronize the frames.

    I'm running following command on windows terminal

    .\rs-convert.exe -i 20230728_180422.bag -p "C:/Users/SOHAM PADHYE/Downloads/png/" -v "C://Users/SOHAM PADHYE/Downloads/png/"

     

    0
    Comment actions Permalink
  • MartyG

    Since SDK version 2.35.0 the rs-convert tool names frame filenames by their timestamp, not the frame number.  Older versions of rs-convert (2.34.0 and older) named the frames by their frame number.

     

    The -v command for csv export is known to not work for some RealSense users.  It appears to have performed the conversion but does not generate any files.  The reason for this is not known and there is not a solution to fix rs-convert's csv export if it does not work for you, unfortunately. 

     

    PNG image file export with -p usually works though.  Is it not generating PNGs for you either?

     

    You can confirm whether the bag file has any problems by playing it back in the RealSense Viewer by drag and dropping the bag file into the center window of the Viewer.

    0
    Comment actions Permalink
  • Sohampadhye1998

    Hello MartyG

    Please help me to get the data at 10fps using realsense ros package.

    I'm getting the the frames at 30 fps. Also tell how to change the frame size.

    0
    Comment actions Permalink
  • MartyG

    10 FPS is not supported for depth by RealSense cameras.  The closest alternatives are 6 FPS (or 5 if using the D455 camera model) or 15 FPS.  If the L515 model is being used then 30 is the only supported FPS for depth.

     

    The only supported mode for 10 FPS that I could find was 1280x720 color on the D455 model.

     

    If you need to set a custom FPS in ROS then you could explore the possibility of setting a rate.

    https://roboticsbackend.com/ros-rate-roscpy-roscpp/

     

    In the RealSense ROS wrapper you can change the resolution by editing the height and width values in the launch file or by defining the custom values in the launch instruction.  For example, to launch with depth and color at 640x480 and 6 FPS:

     

    ROS1

    roslaunch realsense2_camera rs_camera.launch depth_width:=640 depth_height:=480 depth_fps:=6 color_width:=640 color_height:=480 color_fps:=6

     

    ROS2

    ros2 launch realsense2_camera rs_launch.py depth_module.profile:=640x480x6 rgb_camera.profile:=640x480x6

     

     

     

     

     

     

    0
    Comment actions Permalink

Please sign in to leave a comment.