RealSense Support

D455 + T265 3d print mount?

Comments

2 comments

  • Jaa73094

    I noticed the USB port on the D455 is on the bottom. That may lend itself to quite a different mount than the D435, which has the mount on the side. I might see if i can cad up something in Autodesk. These things are pretty simple to make. The only real question is where the coordinate systems and mounting holes are located on the cameras.

    0
    Comment actions Permalink
  • Gbenel

    Thanks, much appreciated!

     

    0
    Comment actions Permalink

Please sign in to leave a comment.