RealSense Support

MacOS Installation Instructions Error

Comments

6 comments

  • MartyG

    Hi Eidsonbrandon  I would recommend following the version of the Mac instructions in the link below, as they are the ones linked to from the front page of the librealsense GitHub site and so will be the most up to date ones:

    https://github.com/IntelRealSense/librealsense/blob/master/doc/installation_osx.md

    0
    Comment actions Permalink
  • Eidsonbrandon

    Hey MartyG,

    I have followed the updated instructions you have linked and am still getting the same error on the same command. 

    Any other ideas? 

     

    Thanks,

    Brandon

    0
    Comment actions Permalink
  • MartyG

    I have not got a Mac to test on, unfortunately, so it is difficult to advise.  If I were building on a non-Mac computer then I would expect the CMake error that you experienced to occur if using the CMake build instruction in an incorrect location. 

    Typically, the CMake build process would involve going to the librealsense root folder of the librealsense source code and doing mkdir build && cd build to create and navigate to a build directory (so you had the path librealsense > build).  Then the CMake command is run from within the librealsense > build folder. 

    Do you have a folder named librealsense, please?

    A couple of years ago there was a Mac installation method posted that more closely resembled the PC one.   It involved cloning the librealsense GitHub to obtain the source code.

    https://github.com/GitwellAnyohub/Real_Sensible_Moseq/blob/master/bash_and_install/install_realsense_sdk_mac_os.sh 

    0
    Comment actions Permalink
  • Eidsonbrandon

    Cloning the librealsense GitHub seems to be the missing piece of info in the previous two guides. As well as navigating to it before creating and populating the build directory. Otherwise, there is no librealsense folder at all. I would suggest updating both the github and website instructions with this info.

    Thank you for your help MartyG! It looks like I am finally set up for development. 

    0
    Comment actions Permalink
  • MartyG

    I am not involved in the documentation.  This case will be a useful reference for future Mac users of RealSense though, and it was a learning experience for myself too.  Good luck with your camera, and please feel free to ask questions!

    0
    Comment actions Permalink
  • Owenplanchart

    @Eidsonbrandon 

    Thank you, this post helped me get to through those unexplained steps. Did you manage to develop with this library at all? I can't seem to open the example files from xcode? 

    0
    Comment actions Permalink

Please sign in to leave a comment.