RealSense Support

D415 - flat surface calibration issues

Comments

4 comments

  • MartyG

    Hi Barry Somers  Having texture for the camera to analyse is important when sensing flat surfaces such as doors, walls, desks, etc.  If the object has no texture or low texture then you can provide that texture by using the camera's projector.  This projects a semi-random pattern of dots onto the scene that the camera can analyse for depth detail.

    Alternatively, if you have a well lit scene then the camera can instead use ambient light in the scene to read depth detail.  The 400 Series cameras actually work better in bright light, which can bring out the depth texture in objects.

    If you are using a D415, the optimal depth sensing resolution for best accuracy is 1280x720

    Intel's excellent camera tuning guide can provide useful guidance for improving image quality if you have not read it already.

    https://dev.intelrealsense.com/docs/tuning-depth-cameras-for-best-performance 

    0
    Comment actions Permalink
  • Barry Somers

    Hi Marty,

     

    Yes we have been using that guide. Thats where we got the textured image from, and will be using next to test in lab this week.

    The 'cameras projector'. Does this refer to the laser emitter? Or is that different? We have tried both with the laser on and off.

    Thanks,

    Barry

    0
    Comment actions Permalink
  • MartyG

    The D415, D435, D435i and D455 camera models have an infrared projector component in them that is separate from the left and right IR sensors.  Yes, it is also known as the IR Emitter.  

    Is the table surface reflective?  If light is projecting onto the table from a nearby light source such as a ceiling light, then reflections generated on the table surface may make those areas more difficult for the camera to read depth data from accurately.  The same phenomenon occurs with reflective floors and floor tiles.

    Section 4.4 of Intel's guide about physical camera filters that can be applied to camera lenses discusses the effect of reflective surfaces and how a linear polarizer filter can improve that situation.

    https://dev.intelrealsense.com/docs/optical-filters-for-intel-realsense-depth-cameras-d400#section-4-the-use-of-optical-filters 

    0
    Comment actions Permalink
  • Barry Somers

    Its not that reflective, but its the only thing we can think of at present to be causing this. That's why we thought maybe textured background will perform better. We will have access to the lab this week so will be testing with textured background and see how that performs.

    We will also experiment more with the external lights in building external to the camera rig, and see how they are affecting the results. Thank you for suggestion.

    0
    Comment actions Permalink

Please sign in to leave a comment.