RealSense Support

Residential Structural Analysis

Comments

1 comment

  • MartyG

    Hi Thedavidgabriel

    I considered your use-case carefully.  I believe that in this case, the L515 may be unsuitable.  Homes tend to have variable lighting and shadow, instead of a consistent light source.  They also have windows, and the L515 can experience interference from IR sources such as sunlight.  In your application, a 400 Series stereo depth camera is likely to be the more suitable choice.  These contain a Vision Processor D4 chip to automatically adjust the camera to changing environmental conditions and can cope excellently with sunlight.

    Of the models available in the 400 Series range, the D435i may meet your needs. It has a wider field of view than the D415 (making it suitable for capturing wide shots of interior views) and a minimum sensing distance of 0.1 meters (compared to 0.4 meters on L515), enabling it to get closer to surfaces.  It contains an IMU component, in case you want to perform SLAM mobile mapping of rooms.   

    https://store.intelrealsense.com/buy-intel-realsense-depth-camera-d435i.html 

    In regard to temperature, the 400 Series can tolerate temperature well.  The bottom of page 43 of the current edition of its data sheet document states that its depth sensing module can bear an official maximum case temperature of 50 degrees C whilst operating.

    The 400 Series has an in-built laser safety mechanism that will halve the laser power if internal temperature exceeds 60 degrees C for several seconds and then shut the laser off if the temperature continues to be excessive.

    Excessive temperature can have a risk of the imaging sensors inside the camera becoming miscalibrated (reducing depth quality and accuracy), though this can be corrected with a software tool.

    The 400 Series data sheet document can be found at the link below:

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet 

    0
    Comment actions Permalink

Please sign in to leave a comment.