Active IR Safety?
Hi,
I noticed that the D415 and D435 are technically Active IR rather than passive. I'm using this in an application that potentially involves explosive or highly reactive substances--is there any particular safety rating or other information about the emitted light from the sensor?
Thank you,
Selam
-
RealSense cameras are a Class 1 laser product that are designed for safe use in industrial applications. Full regulatory information for the product range can be found in the link below.
-
A Class 1 laser should pose no danger to human eye health. The United Kingdom government's website has a good description of Class 1 in Section 5.1 of the document linked to below.
Please sign in to leave a comment.
Comments
3 comments