Behavior of d410 if used in mist atmosphere.
Hi,
Any study on the intel d410 sensor behavior if used in mist atmosphere.
We are trying to use sensor in IP65 enclosure in sub zero condition weather, will sensor have issues.
-
Hi Vikas K R I do not know of a specific study of the 400 Series camera in a mist atmosphere. In general though, you should aim for the operating temperature of the camera to be above 0 degrees C when it is active or the laser's power will cut off.
When the camera is not operating, it should ideally be at 0 degrees C minimum but the data sheet document for the camera says that it can bear a short exposure time of -40 degrees C. The document defines 'short exposure' as representing "temporary max limits acceptable for transportation conditions".
Please sign in to leave a comment.
Comments
1 comment