Vikas K R

  • Total activity 12
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 2

Activity overview

Latest activity by Vikas K R
  • Vikas K R created a post,

    Behavior of d410 if used in mist atmosphere.

    Hi, Any study on the intel d410 sensor behavior if used in mist atmosphere. We are trying to use sensor in IP65 enclosure in sub zero condition weather, will sensor have issues.

  • Vikas K R commented,

    N: Skipping acquire of configured file 'main/binary-armhf/Packages' as repository 'http://realsense-hw-public.s3.amazonaws.com/Debian/apt-repo bionic InRelease' doesn't support architecture 'armhf'

  • Vikas K R commented,

    add-apt-repository "deb http://realsense-hw-public.s3.amazonaws.com/Debian/apt-repo xenial main" -u Traceback (most recent call last):File "/usr/bin/add-apt-repository", line 95, in <module>sp = So...

  • Vikas K R commented,

    its failing here sudo add-apt-repository "deb http://realsense-hw-public.s3.amazonaws.com/Debian/apt-repo xenial main" -u

  • Vikas K R commented,

    how do we install, its failing to install when we follow the steps Page 15 of the user guide for the calibration tools describes how to install the calibration tools package for Debian

  • Vikas K R commented,

    Intel.Realsense.CustomRW.exe is working in windows and we are able to reset to gold calibration, but need to same tool on debian stretch with linux kernel 4.14.79, so we can run on unit that is on ...

  • Vikas K R commented,

    We have already signed NDA with intel. we need to CustomRW software thats works in windows and we use to reset to gold/factory calibration setting. We don't want to recalibrate or create custom cal...

  • Vikas K R commented,

    We have built the SDK in headless debain 8 stretch and using already from past 6 months, we need the customRW to do factory reset in some remote location, since we don't have access to windows PC. ...

  • Vikas K R commented,

    Hi Marty, will this work on raspberrypi, we use headless version? Thanks, Vikas

  • Vikas K R created a post,

    CustomRW on raspbain OS

    Hi,   How to do gold/factory reset on raspbian OS? CustomRW on raspbain OS