RealSense Support

Behavior of d410 if used in mist atmosphere.

Comments

1 comment

  • MartyG

    Hi Vikas K R  I do not know of a specific study of the 400 Series camera in a mist atmosphere.  In general though, you should aim for the operating temperature of the camera to be above 0 degrees C when it is active or the laser's power will cut off. 

    When the camera is not operating, it should ideally be at 0 degrees C minimum but the data sheet document for the camera says that it can bear a short exposure time of -40 degrees C.  The document defines 'short exposure' as representing "temporary max limits acceptable for transportation conditions".

    0
    Comment actions Permalink

Please sign in to leave a comment.