RealSense Support

Urgent: Need help: Binary image (to generate ROI) from Depth information D435

Comments

6 comments

  • MartyG

    The link below provides C++ scripting for saving a binary image file (.bin) and discusses how the code works.  I hope that it will be helpful to you.

    https://github.com/IntelRealSense/librealsense/issues/1485  

    I wonder if using the RealSense SDK's auto-exposure ROI function would satisfy your needs.  It averages the intensity of the pixels within the ROI and tries to maintain them at a pre-defined "setpoint" level.

    A C++ code example for setting the auto-exposure ROI is here:

    https://github.com/IntelRealSense/librealsense/issues/4363#issuecomment-508405760 

    If you would like to test setting an auto-exposure ROI with the RealSense Viewer program by drag-selecting an area of the image, page 2 (section 2e) of Intel's excellent camera tuning guide describes how to do so.

    https://www.intelrealsense.com/wp-content/uploads/2019/11/BKMs_Tuning_RealSense_D4xx_Cam.pdf  

    In regard to checking depth values so that they are not < 0, I wonder if you could adapt the depth value checker code in the rs_align_advanced sample program in the link below, so that if pixel distance < 0 then pixel distance = 0 (instead of cutting the pixel off).  That way, invalid / NaN value pixels would still be represented in the data as '0'.

    https://dev.intelrealsense.com/docs/rs-align-advanced 

    A similar technique could be used to say that if a pixel distance is > 0 then the pixel distance = 1. 

    The code is at the bottom of the sample program's page.

    0
    Comment actions Permalink
  • Smartstartup1081

    Thanks @MartyG will try this out and update the thread

    0
    Comment actions Permalink
  • Smartstartup1081

     

    From reference cpp - Tried above code (python) - But hitting below error - I am getting depth_image as Numpy array - not single value...How should I proceed..please help

    ERROR:

    if (pixel_dist <= 0.0 or pixel_dist > 1.828):
    ValueError: The truth value of an array with more than one element is ambiguous. Use a.any() or a.all()

     

    By the way I am not looking for " auto-exposure ROI" - Objective is to generate Binary image - White pixels covering area occupied by any objects with depth - all other pixels to Black...

    0
    Comment actions Permalink
  • MartyG

    My Python programming skills are not currently advanced enough to write my own solution, but I did find some Python programming advice on the link below that may be helpful.

    https://stackoverflow.com/questions/34472814/use-a-any-or-a-all 

    0
    Comment actions Permalink
  • Smartstartup1081

    Able to solve the problem with OpenCV threshold 

    -> Convert RGB to Gray

    -> Do Gaussian blur

    -> Apply OTSU threshold on blur image - This will give you binary image

     

    Thank you  for the support MartyG

     

    0
    Comment actions Permalink
  • MartyG

    Great news that you found a solution - thanks for sharing your method with the RealSense community!

    0
    Comment actions Permalink

Please sign in to leave a comment.