RealSense Support

Xeon E3-1230 V2

Comments

2 comments

  • Hillsh 47

    Sorry, meant to type Xeon E3-1230 V2

    0
    Comment actions Permalink
  • MartyG

    The original SR300 model from 2016 had strict limitations on the processors that it would work with, and it had only a 50% chance of working on a Xeon V5 generation from around 2016.  Your V2 processor is from 2012. 

    Having said that, I believe that the limitations were imposed by the software SDK of the time rather than the hardware.  The modern 2019 data sheet document for the SR300 and SR305 only states a USB 3 port as a hardware requirement (the SR30x cameras cannot use USB2) and a minimum OS of Ubuntu 16 or Windows 10 as a software requirement.

    0
    Comment actions Permalink

Please sign in to leave a comment.