View my account

D435 left IC2 error

Comments

5 comments

  • MartyG

    Could you check the connection between the D430 Depth Module board and the Vision Processor board to see if they are firmly attached? 

    Are you using the rigid connector board or a flexible cable to make the connection between the two?

    0
    Comment actions Permalink
  • 050799rmm

    I have connected the camera with the original type c cable from the box.

    0
    Comment actions Permalink
  • MartyG

    The D430 is a camera circuit board module without a casing.

     

     

    Did you mean that you have a D435 camera, please?

     

    0
    Comment actions Permalink
  • 050799rmm

    Yes, sorry, it's a d435...

     

    0
    Comment actions Permalink
  • MartyG

    Okay, thank you very much.  I believe that IC2 errors are an error with the camera hardware.  If you can access the RealSense Viewer program, does the error get connected if you go to the 'More' icon at the top of the Viewer's options side-panel and select the 'Hardware Reset' option from its menu?

    If you do not have the RealSense Viewer, you can achieve the same reset by unplugging the camera, waiting a couple of seconds and then plugging it back into the USB port with a quick, firm insertion action.

    0
    Comment actions Permalink

Please sign in to leave a comment.