RealSense Support

Intel publish white paper on high speed 300 FPS depth capture for D435

Comments

10 comments

  • Ozaki

    Dear Sirs:

    Where can I find the firmware version 5.12.4.0?

    I could not find it in

    https://dev.intelrealsense.com/docs/firmware-releases.

    The site has the version up to 5.12.3.

    Thanks.

    Oz

    0
    Comment actions Permalink
  • MartyG

    Firmware releases are normally listed on the page in the link below, but a 5.12.4.0 version is not listed yet.

    https://dev.intelrealsense.com/docs/firmware-releases 

    0
    Comment actions Permalink
  • Ozaki

    Thak you, Marty.

    In the whitepaper, it says,

    2. How to enable high-speed capture mode

    The high-speed depth capture is enabled in firmware version 5.12.4.0 or later. It can be downloaded from the Intel RealSense website [1].

     

    So I would like to test the high-speed capture mode with the firmware version 5.12.4.0.

    Anyway, I will wait for it.

    Thanks,

    Oz

    0
    Comment actions Permalink
  • MartyG

    Sometimes the mention of a new firmware version comes before its actual availability on the firmware downloads page.  Thanks for your patience!

    0
    Comment actions Permalink
  • Sergipanadero

    Any news on when the firmware update 5.12.4 will be released?

    0
    Comment actions Permalink
  • MartyG

    Firmware version 5.12.5.0 has been available since yesterday.  It is not available as an individual download on the firmware releases page yet at the time of writing this message but can be updated to from the RealSense Viewer program within the new 2.35.0 version of the RealSense SDK.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.35.0 

     

    To update to this firmware from within the RealSense Viewer version of SDK 2.35.0 after installing this new SDK, launch the program and go to the 'More' option at the top of the Viewer's options side-panel, and select 'Install Recommended Firmware' from its drop-down menu.

    1
    Comment actions Permalink
  • Aeaa5023

    Is High-speed capture mode enabled in firmware 5.12.5?

    0
    Comment actions Permalink
  • MartyG

    Aeaa5023  It seems so.  The firmware release notes for 5.12.5 state that "the release also includes support for 256x144 @ 300FPS and 848x100 @ 300FPS formats for D43x cameras".

    0
    Comment actions Permalink
  • Akmaldeen20

    Is it possible to get frame 300fps in D455 camera ? 

    0
    Comment actions Permalink
  • MartyX Grover

    Hi Akmaldeen20  I tested the D455 in the RealSense Viewer program at 848x100 depth but could only select 100 FPS maximum at the time of writing this.  The D435i model was able to successfully stream 848x100 depth at 300 FPS in the Viewer.

     

     

    1
    Comment actions Permalink

Please sign in to leave a comment.