RealSense Support

Multiple Camera Support of D4 VPU / RGB Calibration on D430 Module

Comments

5 comments

  • MartyG

    1.  A RealSense integrator who was constructing their own design from individual parts said "From my understanding these (the imagers) are just standard MIPI CSI-2 camera modules (OV9821 and OV2740), so any modules with similar spec (MP/s, etc.) should work".

    The free public version of the calibration software for the 400 Series cameras can only calibrate extrinsics though.  To calibrate both extrinsics and intrinsics, an OEM version of this software is required.  The easiest way to obtain this software is to purchase the $1500 USD "OEM Calibration Target" system from the official RealSense Store.  This large-scale calibration board, which is aimed at engineering departments and manufacturing facilities, is designed for calibrating multiple RealSense cameras and enables connection to cameras through a remote Linux server.

    https://store.intelrealsense.com/buy-intel-realsense-d400-cameras-calibration-target.html 

    Camera calibrations can be written to flash memory storage on the the camera hardware.  The data sheet document for the 400 Series cameras states that the EEPROM where the calibration data is stored is on the Depth Module, not the Vision Processor D4.

    2.  Usually, one Depth Module board is paired with one Vision Processor D4 Board.  I have not come across setups where multiple Depth Module boards are associated with a single Vision Processor D4 Board.  The product brief for the D4 suggests that it is talking about connection of up to 5 MIPI CSI-2 camera imager modules, not five complete cameras.

    https://www.mouser.mx/pdfdocs/Intel_Vision_Processor_D4_ProductBrief.pdf 

    3.  The links below have guides to using the 400 Series cameras with ROS using 2-camera and 3-camera setups.  I hope that these will help to answer this question.

    https://github.com/IntelRealSense/realsense-ros/wiki/Showcase-of-using-2-cameras

    https://github.com/IntelRealSense/realsense-ros/wiki/showcase-of-using-3-cameras-in-2-machines 

    For expert advice on ROS, I recommend posting your questions on the RealSense ROS GitHub forum by visiting the link below and clicking the 'New Issue' button.

    https://github.com/IntelRealSense/realsense-ros/issues 

    1
    Comment actions Permalink
  • MartyG

    I should add that "D435" refers to the cased USB camera.  If you are seeking to build a camera system from separate components then you will need the D430 Depth Module.  The D430 is the name of the camera board inside the D435's casing.

    1
    Comment actions Permalink
  • Kyuman Lee

    Yes, you're right. I was asking about a D430 module.

    0
    Comment actions Permalink
  • Kyuman Lee

    I have follow-up questions.

    1. When changing a custom RGB camera on an Intel D430 module, how can I set the intrinsic & extrinsic parameters of the custom RGB camera on the D430 module?

    Why is "OEM Calibration Target" system too expensive? Even though I purchased Depth Module D430 + Vision Processor D4 Board Bundle (10 Pack), do I need to purchase the OEM software as well to calibrate each RGB camera sensor per module?

    Is the EEPROM the flash memory storage on the camera hardware module to store the intrinsic & extrinsic parameters of the custom RGB sensor and depth sensors? 

    0
    Comment actions Permalink
  • MartyG

    The cost of the OEM Target Board is mostly the cost of manufacturing the physical board.  As far as I know, the only other way to get the OEM software is if you have a Non Disclosure Agreement (NDA) relationship with Intel, which can be difficult to qualify for.  So the OEM board is the easier way to obtain the software.

    I believe the reason why the free version does not support intrinsics calibration is that Intel believe that calibrating the extrinsics has much more effect on the camera image than changing the intrinsics does. 

    I have not heard of anyone who was constructing their own camera from the Depth Module and D4 feeling the need to purchase the OEM Target board too, unless it was for the reasons of calibrating multiple cameras or using the OEM system's ability to connect to cameras remotely via a Linux server.

    According to the data sheet document the EEPROM on the depth module stores the calibration data, yes.  RGB can be calibrated if the device supports it.  My understanding is that the firmware driver detects a D430 without RGB as 'D430' but identifies it as 'D435' if an RGB imager is detected as being connected.

    Details of how the Dynamic Calibrator handles RGB calibration can be found in its PDF user guide.  If you search the document for 'rgb' then it makes it easy to browse through all the parts where RGB calibration and the writing of its data is discussed.

    https://www.intel.co.uk/content/www/uk/en/support/articles/000026723/emerging-technologies/intel-realsense-technology.html 

    0
    Comment actions Permalink

Please sign in to leave a comment.