RealSense Support

D435 Recommended firmware

Comments

3 comments

  • MartyG

    In the absence of a recent Production firmware, a good rule of thumb for a stable production build is "one version back" from the latest version.   That goes for RealSense SDK versions too.  By using one version back, you help to ensure stability by giving time for problems that may arise from the latest versions to be addressed with fixes.  

    So under a "one version back" guideline, the following versions would apply:

    SDK: 2.32.1

    FIRMWARE: 5.12.2.100

    0
    Comment actions Permalink
  • Shigeyoshi Ohara

    Hello,

    The information of recommended configuration seems not be updated for long time. May I ask if it is still the latest information?

    https://dev.intelrealsense.com/docs/recommended-production-camera-configurations

     

    Regards

    0
    Comment actions Permalink
  • MartyG

    Hi Shigeyoshi Ohara  The recommended production configuration is useful as a specification for a proven setup that you can feel confident in putting into a commercial product or critical application that uses RealSense.

    If you would prefer to test a newer configuration in such a project then a good rule to apply may be "one version back" - using an SDK and firmware version that is one version older than the current most recent versions.  Doing so provides the opportunity to see whether there are any issues that arise from a new release.

    0
    Comment actions Permalink

Please sign in to leave a comment.