View my account

I can't start Viewer for d415 on wins 10

Comments

1 comment

  • MartyG

    If programs bundled with the RealSense SDK such as the RealSense Viewer and Depth Quality Tool will not launch or freeze on launch, it can be an indicator of a problem with the OpenGL graphics drivers on a computer, as these programs use OpenGL to display the graphics.

    If the graphics chip (GPU) in your computer supports OpenGL (which it should do if they are a mainstream GPU brand such as Nvidia or Intel) then updating the graphics drivers on your computer may make the Viewer work.

    0
    Comment actions Permalink

Please sign in to leave a comment.