RealSense Support

Ubuntu 16.04 LTS: realsense-viewer can not recognize D435i after firmware update failed

Comments

3 comments

  • MartyG

    If the camera is working fine on the Jetson Nano then the problem is probably not related to the firmware driver.  The firmware is stored inside the camera and not on the PC, so any problem with the firmware that stops the camera from working would be transferred to any other computer that the camera was connected to.

    Does the camera work on the Up Squared if you do a total shutdown (not a restart) of the Up Squared board and then boot the Up again from shut-off, please?

    0
    Comment actions Permalink
  • Baiyu0584

    Just like you suggested, after a total reboot it works.Thanks a lot!

    0
    Comment actions Permalink
  • MartyG

    That's great news.  Thanks for the update!

    0
    Comment actions Permalink

Please sign in to leave a comment.