need 3D model or step file for the D415 interposer PCB board 82635DSITR50P
pls provide the 3D model for the D415 interposer PCB board which has two 50 pin connectors on it, part number is 82635DSITR50P. thanks very much
-
There is not an official or unofficial CAD file for the 400 Series interposer board product, unfortunately. I carried out an extensive search for details but all technical enquires about the board are directed to the general data sheet document for the 400 Series.
https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet
The component retailer Mouser listed the dimensions of the board if you would like to use that as the basis for creating your own model:
89.7 mm x 10 mm x 4.7 mm
-
Here is an un-official model of the 82635DSITR50P created from some measurements and guesses. Use at your own risk.
https://github.com/PowersConsulting/RealSenseInterposer/raw/Model.82635DSITR50P/Interposer.stepThe main branch of that repository (https://github.com/PowersConsulting/RealSenseInterposer/tree/master) has an untested Altium design for a very similar board which would have 10mm center-to-center connector measurements and should be able to be manufactured on low-cost PCB basis. PRs/forks welcome. Hope these are useful to someone :D
Please sign in to leave a comment.
Comments
5 comments