View my account

need 3D model or step file for the D415 interposer PCB board 82635DSITR50P

Comments

5 comments

  • MartyG

    There is not an official or unofficial CAD file for the 400 Series interposer board product, unfortunately.  I carried out an extensive search for details but all technical enquires about the board are directed to the general data sheet document for the 400 Series.

    https://dev.intelrealsense.com/docs/intel-realsense-d400-series-product-family-datasheet 

    The component retailer Mouser listed the dimensions of the board if you would like to use that as the basis for creating your own model:

    89.7 mm x 10 mm x 4.7 mm

    0
    Comment actions Permalink
  • Robert

    The dimensions of 82635DSITR50P are about 10mm X 10mm. The center-to-center distance between the two connectors is 7.5mm.

    Source: Bought some and measured them.

    0
    Comment actions Permalink
  • MartyG

    Thanks very much for your correction Robert.  The 89.7 mm figure above seems to be taken from the total width of a depth module board, which would not make sense for the interposer board's dimensions as it is shown to be a square shape rather than a rectangle!  Thanks again. :)

    0
    Comment actions Permalink
  • Robert

    Here is an un-official model of the 82635DSITR50P created from some measurements and guesses. Use at your own risk.
    https://github.com/PowersConsulting/RealSenseInterposer/raw/Model.82635DSITR50P/Interposer.step

    The main branch of that repository (https://github.com/PowersConsulting/RealSenseInterposer/tree/master) has an untested Altium design for a very similar board which would have 10mm center-to-center connector measurements and should be able to be manufactured on low-cost PCB basis. PRs/forks welcome. Hope these are useful to someone :D

     

    0
    Comment actions Permalink
  • MartyG

    Great assets, Robert - thanks again for sharing this excellent contribution with the community!   I will post a link to your message at the RealSense GitHub forum so that a greater number of RealSense users can discover it.

    0
    Comment actions Permalink

Please sign in to leave a comment.