Multiple Realsense L515 cameras
I have a few questions about this product:
Is there any issue with operating multiple Realsense L515 cameras in the same environment? In other words, do they interfere with each other?
If they can be used near each other, is there a way to sync multiple units connected to the same computer so that that they take their pictures at the same time?
Finally, part of building a reliable system with multiple cameras is being able to tell one from another. Do these cameras have unique serial numbers that can be read by the host computer?
-
The L515 supports multi-camera synchronization. The official L515 FAQ says "Multiple cameras can share the same field of view utilizing our hardware sync feature". Dorodnic the RealSense SDK Manager has said that the sync connector is not the same as the one on the 400 Series cameras but is similar.
I do not yet have information on your other questions unfortunately. The best place to ask would be on the announcement post for the L515 on the RealSense GitHub site,
https://github.com/IntelRealSense/librealsense/issues/5430
Regarding the serial number query though, the RealSense ROS wrapper now has the option of communicating with a specific device by USB port ID instead of the device's serial number.
Please sign in to leave a comment.
Comments
1 comment