RealSense Support

Multiple Realsense L515 cameras

Comments

1 comment

  • MartyG

    The L515 supports multi-camera synchronization.  The official L515 FAQ says "Multiple cameras can share the same field of view utilizing our hardware sync feature".  Dorodnic the RealSense SDK Manager has said that the sync connector is not the same as the one on the 400 Series cameras but is similar.  

    I do not yet have information on your other questions unfortunately.  The best place to ask would be on the announcement post for the L515 on the RealSense GitHub site,

    https://github.com/IntelRealSense/librealsense/issues/5430

    Regarding the serial number query though, the RealSense ROS wrapper now has the option of communicating with a specific device by USB port ID instead of the device's serial number.

    https://github.com/IntelRealSense/librealsense/issues/5118 

    0
    Comment actions Permalink

Please sign in to leave a comment.