RealSense Support

SR300 firmware updated and is now detected as SR305

Comments

4 comments

  • MartyG

    Assuming that the scanner was not using a special version of the SR300 firmware, the best way to overwrite an older firmware would likely be to download the SR300 Depth Camera Manager (DCM).  The SR300 DCM file (intel_rs_dcm_sr300_3.3.27.5718.exe) can be found at the bottom link in the side-panel of the page linked to below.

    https://downloadcenter.intel.com/download/25044/Intel-RealSense-Depth-Camera-Manager

    Running the DCM program (which requires Windows and will not work with Linux) normally installs all SR300 drivers (the firmware, plus the RGB, Depth and Virtual drivers).  

    If you do not want to install every driver, there is a process where you can force the DCM to only install the firmware, though it is a bit awkward.  A member of the Intel RealSense support team posted a method for force-updating the R200 camera that belongs to the same generation of camera models as the SR300.

    https://github.com/IntelRealSense/librealsense/issues/1731#issuecomment-393070112

    In the step that uses the filename intel_rs_dcm_r200_xxx.exe try intel_rs_dcm_sr300_xxx.exe instead

    In the step that say to run FWUpdateR200.exe, run FWUpdateSR300.exe instead

    0
    Comment actions Permalink
  • Sherrill Ryan

    Thank you for the quick response.  I have already tried to install the SR300 DCM.  It will not install because the computer does not see a SR300.

    There is an option in the RealSense Viewer to update firmware from file.  That seemed like it would be pretty easy, but maybe not.

    I will let you know how it goes after I try your suggested method.

    0
    Comment actions Permalink
  • Sherrill Ryan

    I was able to get it to work.  I extracted the DCM per the instructions.  The next step did not work for me.  However, I was able to find the signed firmware image in the extracted information and load that using the RealSense Viewer.

    Thank you for your help!

    0
    Comment actions Permalink
  • MartyG

    Awesome news!  I'm very glad you were able to restore.  :)

    0
    Comment actions Permalink

Please sign in to leave a comment.