Pose estimation error on PITCH and ROLL
Hi, I am using two Realsense t265 on a windows machine, through the python binding.
I have huge problems understanding the data...
The data you see in he figures are YAW, PITCH and ROLL for 2 devices, that are attached together on a plate. The task is walking on a rectangular path (about 60x45 feet) with the cameras sitting on a chair with wheels. So it is 4 turns, each of 90 degrees in the same direction.
As you can see, the YAW data are quite good and the 2 sensors are quite aligned each other.
There are a lot of problems on the PITCH and ROLL:
- they should be almost steady since we are not really changing them
- they jump from 0 to +180 or -180 degrees
- they jump differently each other
- during and after the turn there is a relevant misalignment between the two sensors, which is not a multiple of 180, but it is roughly between 10 and 30 degrees.
Can you help me understanding what is going on?
Thank you,
Agostino
-
For expert advice on very technical T265 questions, I recommend re-posting your question and the accompanying images at the RealSense GitHub forum. You can do so by visiting the link below and clicking the 'New Issue' button. Thanks!
Please sign in to leave a comment.



Comments
2 comments