RealSense Support

Use of SR305 in special light conditions

Comments

1 comment

  • MartyG

    For bright-light conditions, a 400 Series model (D415 or D435 / D435i) may be the better choice.  Unlike most depth cameras, these stereo cameras actually work better in strong light. 

    If you are referring to a pattern projector that overlays a pattern of dots onto the scene: in strong light, a pattern projector is not needed because the 400 Series cameras can use the ambient light of the scene for reading depth detail instead.  Its auto-exposure can also adjust to variable lighting conditions such as daylight and darkness in real-time.

    0
    Comment actions Permalink

Please sign in to leave a comment.