RealSense Support

Distance to Target on D415 (Python)

Comments

5 comments

  • MartyG

    If you are okay with recording the data into a 'bag' file first instead of doing the calculations on live-streams, Intel's Python 'Distance to Object' tutorial may meet your needs for calculating the distance to an object.

    https://github.com/IntelRealSense/librealsense/blob/jupyter/notebooks/distance_to_object.ipynb 

    If you prefer to use live-streams, code for setting the auto-exposure ROI in Python can be found here:

    https://github.com/IntelRealSense/librealsense/issues/2681#issuecomment-436391721 

    Another approach to a region of interest is to crop the X and Y of the image so that only data within a 'bounding box' is considered.  This is more complicated to implement.

    https://github.com/IntelRealSense/librealsense/issues/4838 

    You can enhance the image by applying post-processing filters to it.  An Intel tutorial for doing this in Python is here:

    https://github.com/IntelRealSense/librealsense/blob/jupyter/notebooks/depth_filters.ipynb 

    0
    Comment actions Permalink
  • Shop4gk

    Thanks for your quick and extremely useful response. I shall look into these and try to implement the most suitable way to solve my problem.

    If you don't mind, I would like to further pick your brain as to why should there be a need for a bounding box if my target covers the whole camera field of view. Why am I getting values like zero and extremely high values when the target is <1 m away. I am inclined to think that it is noise since the average of all pixels of the depth image yields a value that is somewhat near to my target distance. In which case, is there a way to eliminate the noise pixels in my depth image, by averaging multiple frames (for now my target and camera are static).

    Thanks again!

    0
    Comment actions Permalink
  • MartyG

    With the 400 Series stereo cameras, the error factor (RMS error) increases over distance.  It is very small at close range to an observed object but accumulates linearly as the object becomes further away.  The error factor starts to become noticeable when further than 3 meters away.

    For some people the error factor is problematic at > 1 depending on how precise they need their measurements to be (e.g even 4 mm error is unacceptable to their project).

    RMS error can be reduced by around 30% by turning off the IR Emitter (the component that projects a semi-random pattern of dots onto the scene to enhance the readability of low-detail surfaces such as walls, doors and desks).  In a well-lit scene, the camera can use ambient light to calculate depth instead of the dot projection.

    If you feel you need a dot pattern projection, using an external LED projector instead of the camera's built-in laser based projector can reduce 'laser speckle' noise on the image.

    If you get depth values of zero, this may represent detail in the scene that the camera is unable to read for some reason.   This may include environmental factors such as reflections on an observed surface, or the surface being dark grey / black (this color absorbs light). 

    You may also experience greater noise at the left side of the image due to a phenomenon called 'invalid depth band'.  This is described on pages 58-59 of the current edition of the 400 Series data sheet document.

    https://www.intel.co.uk/content/www/uk/en/support/articles/000026827/emerging-technologies/intel-realsense-technology.html 

    0
    Comment actions Permalink
  • Shop4gk

    Thanks for the insight! My target is going to be less than 2 meters away so the distance is definitely not an issue. I will try to experiment in bright sunlit area and get back in case of any further issues being faced. My whole problem seems to be boiling down to the difference between the way the Depth Quality Tool seem to be calculating the distance and the way it is being exposed through the Python wrapper. I need to dig deeper into it.

    Cheers!

    0
    Comment actions Permalink
  • MartyG

    You are very welcome!  

    If you are in an office environment, fluorescent lights such as ceiling strip-lights may negatively impact the image due to gas inside the lights flickering at frequencies hard to see with the human eye.  If you have such lights in the room, using a camera FPS close to the operating frequency of the lights (30 FPS for some lights, 60 FPS for others) may help.

    Good luck!

    0
    Comment actions Permalink

Please sign in to leave a comment.