View my account

Conflict between RealSense Viewer (2.20 and up) and card reader with USB over IP

Comments

3 comments

  • Alexandra Ciuriuc

    Hello Diogo,

     

    Thank you for your interest in the Intel RealSense D435 camera.

    Did you test this on a different computer? Do you see the same issue?

     

    Regards,

    Alexandra

    0
    Comment actions Permalink
  • Diogo Frutuoso

    Hello Alexandra,

    Yes, I did try on a different PC and even with a different card reader (model).

    The issue really seems to be related with the USB over IP reason why I was trying to figure out if something related with the USB connection changed on SDK version 2.20 and up. What puzzles me the most is that I don't even need to have the camera connected, just the RealSense viewer running and the problem is present.

    I'm assuming the issue is only related with the RealSense SDK only because from the card reader point of view, nothing has changed, firmware or software.

    Best regards.

    0
    Comment actions Permalink
  • Alexandra Ciuriuc

    Hello Diego,

     

    I tested this with the latest librealsense version and a USB 3 card reader. It worked with no issues, with the camera connected, while streaming.

    This might a network issue, you should check it. 

     

    Regards,

    Alexandra

    0
    Comment actions Permalink

Please sign in to leave a comment.