RealSense Support

Cables/Adapters for SR305

Comments

1 comment

  • MartyG

    Historically, RealSense cameras have always been sensitive to the state of the USB port / cabling, no matter the model.  This is because of the high volume of data that they typically transmit through the cable, which reduces the distance that the data can be sent along before it degrades unless a high-quality cable is used.

    Newnex does have an A male to Micro B male cable with screw lock for SR305 and T265 that is mentioned in their RealSense promo page on their site.

    https://www.newnex.com/realsense-3d-camera-connectivity.php 

    The cable referenced for SR305 and T265 is accessible here:

    https://www.newnex.com/usb-3-locking-cables.php#USB3LockingAtoMicroB 

    If you scroll down the page then cables with lengths up to 5m are available.

    0
    Comment actions Permalink

Please sign in to leave a comment.