SR305 Camera is detected as SR300 and acts weird
SR305 suddenly acts weird. Depth stream image is blue. Camera is detected of SR300. I would like to update with Firmware of SR305. Where cane I find the firmware? Can someone one post the firmware? Thank you.
-
The SR300 and SR305 firmware can be updated with the More option at the top of the RealSense Viewer options side panel or with the rs-fw-update tool.
If you select the 'Install Recommended Firmware' option then the Intel-recommended firmware will be automatically installed without you having to go find the firmware file, as the recommended file is bundled into the RealSense Viewer.


https://github.com/IntelRealSense/librealsense/issues/4755#issuecomment-527216341
Please sign in to leave a comment.
Comments
1 comment