RealSense Support

SR305 Camera is detected as SR300 and acts weird

Comments

1 comment

  • MartyG

    The SR300 and SR305 firmware can be updated with the More option at the top of the RealSense Viewer options side panel or with the rs-fw-update tool.

    If you select the 'Install Recommended Firmware' option then the Intel-recommended firmware will be automatically installed without you having to go find the firmware file, as the recommended file is bundled into the RealSense Viewer. 

    https://github.com/IntelRealSense/librealsense/issues/4755#issuecomment-527216341

    0
    Comment actions Permalink

Please sign in to leave a comment.