RealSense Support

Regarding D415 Calibration in Vertical Direction

Comments

1 comment

  • MartyG

    The D415 has been used successfully to measure depth when pointed downwards towards the floor.  So I would imagine that if the camera is calibrated in the normal front-facing orientation then it should not make a difference if you then point the camera upwards during use.

    An exception to this is calibrating an IMU component in a RealSense camera such as the D435i, which apparently must be calibrated in the forward-facing horizontal direction.  That does not apply here though, since the D415 does not have an IMU.

    0
    Comment actions Permalink

Please sign in to leave a comment.