Rsharma2

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 2
  • Subscriptions 2

Activity overview

Latest activity by Rsharma2
  • Rsharma2 commented,

    Hi, Thank you for the comments. As per your suggestion, I replaced the D435 with D415 and the results are better. But still, I needed to tune the depth control parameters given in the Advanced Cont...

  • Rsharma2 created a post,

    Regarding D415 Calibration in Vertical Direction

    Hi, I wanted to scan the D415 placed vertically to utilise the lesser Horizontal FOV from LIPScan, that is, I wanted to turn the camera vertically and then calibrate it for accurate measurement. Ho...

  • Rsharma2 commented,

    Thank you for the info! One more thing: is there any object size and feature limitations because the object which I'm scanning is a small fan with many edges, and it's not able to recognise the dep...

  • Rsharma2 created a post,

    Regarding D435 Object Scanning Limitations

    Hi, I'm trying to 3-D scan an object of size approx. 10cm * 10cm * 3cm which is circular symmetric using a turntable. The software which I've been using for this is RecFusion. I had two questions: ...