RealSense Support

Dimensional Analysis of an object using realsense D435

Comments

15 comments

  • MartyG

    Hi Darkdevelopers6710 The RealSense SDK has a Python box measuring example project called box_dimensioner_Multicam.  Despite the name, it can be used with a single camera like in your setup in the images above.

    https://github.com/IntelRealSense/librealsense/tree/master/wrappers/python/examples/box_dimensioner_multicam

     

     

    The box_dimensioner_multicam has a 'sweet spot' distance of around 0.5 meters that provides best results.  If the camera is nearer or closer than that then the green bounding box (shown above) that is overlaid on the RGB color image can be wrongly oriented and the measurements may be inaccurate. It uses depth information by calculating a point cloud

     

     

    Although the project requires the box to be placed on a checkerboard image, it is possible to edit the project's code to remove the need for the box if you are using a single camera.

     

    Usually the camera is placed at the corners of the checkerboard and angled diagonally towards the box instead of being placed directly above the box pointing downwards.

     

     

    1
    Comment actions Permalink
  • MartyG

    If you are able to use a pre-existing commercial software solution then object dimensioning software by a company called MobileWorx might meet your needs.  It enables objects such as boxes to be measured with a tablet that has a RealSense 400 Series camera attached to its rear, inserted into a rubber boot.

    https://www.mobileworxs.com/xdim-mobile-dimensioning-software/

    1
    Comment actions Permalink
  • Yoges It Tech

    Hi MartyG Thanks for your detailed explanation and the effort. The link you shared is very helpful for two cameras. Is there any package or library to detect with a single camera? Please suggest.

    2
    Comment actions Permalink
  • MartyG

    Do you mean the box_dimensioner_multicam link?  If you do then that project works with a single camera.

    1
    Comment actions Permalink
  • Yoges It Tech

    Yes, we need to do with Single camera.

    1
    Comment actions Permalink
  • MartyG

    Hi Yoges It Tech  Are you a different person to Darkdevelopers6710 who created this discussion, please?

    1
    Comment actions Permalink
  • Yoges It Tech

    Me and Darkdevelopers6710 are working on the same project. MartyG

     

    0
    Comment actions Permalink
  • MartyG

    Thank you very much for the clarification.

     

    box_dimensioner_multicam will work with a single camera.  It is the best open-source solution available for box measuring with a RealSense camera.  Because box_dimensioner_multicam and the RealSense SDK are open-source and can be freely modified, you could use them as the foundation for your own project.

     

    In regard to commercial pre-made solutions, in addition to the Mobileworx system mentioned above, another dimensioning tool that is powered by the RealSense D455 camera model is xDIM Mobile Dimensioning

    https://4dmobilesoft.com/

    0
    Comment actions Permalink
  • Yoges It Tech

    Hi MartyX Grover

    Thanks for the suggestion.

    Please clarify the following questions:

    1. Where and what parameters/code should I change to make the multicam configuration to a singlecam one?

    2. While I am on the single cam config, at what degree should I place my camera when compared to the mean position (top facing)?

    3. Chessboard corners are not being detected. What could be the issues? Is it just the single cam config or is there something else?

    0
    Comment actions Permalink
  • MartyG

    1.  box_dimensioner_multicam can be used with a single camera without having the modify the parameters.  

     

    If you wish to use a larger chessboard image than 6x9" though then you will need to modify square size parameters in the code.

     

    If you would prefer not to have to use a chessboard then the link below has a discussion about modifying the project to use the intrinsic parameters of a single camera instead of using a checkerboard to calculate this information.

    https://github.com/IntelRealSense/librealsense/issues/10054

     

    2.  There is not a recommended tilt angle.  In the two-camera image that I provided earlier though, it looks as though the cameras are angled at around 45 degrees.

     

     

    If you are testing box_dimensioner_multicam, do you have the camera positioned at the corner of a 6x9" chessboard, looking diagonally towards the center of the chessboard and mounted at a distance of around 0.5 m from the board?  Is the green bounding box correctly displayed around the box?

     

    box_dimensioner_multicam calculates the chessboard corners but is not meant to display that information to the user.

    0
    Comment actions Permalink
  • Yoges It Tech

    Okay Thanks for the information MartyG

    0
    Comment actions Permalink
  • Yoges It Tech

    Hi MartyX Grover,

    I made the code work by doing some slight modifications and got great results with cuboidal objects. Moving forward, I have some queries that I couldn't resolve.

    1. How can I make the cuboidal-bounding box shapeshift? For example, if there is a cylinder shape object, how can I make my bounding box trace the edges of that object (like a polygon bounding box)?

    2.  Is there some way I could tweak the code in order to make the program detect for cavities or holes in the object? Also how can I measure the depth of the cavity?

    0
    Comment actions Permalink
  • MartyG

    A possible approach for creating a bounding box for irregularly shaped objects is to use OpenCV contour code to form a bounding around the object from rectangles and circles.

    https://docs.opencv.org/3.4/da/d0c/tutorial_bounding_rects_circles.html

     

    In regard to detecting holes, a viable OpenCV approach may be to use a canny edge detection algorithm to find holes.

    https://answers.opencv.org/question/173326/how-to-find-coordinates-of-holes/

    https://github.com/IntelRealSense/librealsense/issues/7364#issuecomment-727635090

     

    Checking the depth of holes could be difficult if the holes are small as they may not stand out enough from the surface to be recognized as separate from the overall surface.

    https://support.intelrealsense.com/hc/en-us/community/posts/360038418393-I-have-to-use-an-intel-realsense-d435i-to-check-the-existence-of-contaminants-in-concrete-slabs-with-recesses-for-hoses-Which-parameters-of-the-d435i-do-I-have-to-configure-

    0
    Comment actions Permalink
  • Murali D

    Hi MartyG,


    Have trying same solution, one info would like to know that, is this solution would work with any other camera instead of Intel RealSense DXXX camera with SDK 2.0 ? 

    Thanks,

    Murali. 

     

    0
    Comment actions Permalink
  • MartyG

    Hi Murali D  I can only advise about Intel RealSense cameras, not other types of camera.

    0
    Comment actions Permalink

Please sign in to leave a comment.