RealSense Support

What type of glue for placing IR filer to D 415 camera

Comments

1 comment

  • MartyG

    Hi Karin Dijkstra  A RealSense user once used rubber bands instead of glue to hold an external ND filter to the front of the camera, so that solution may be worth considering if the camera does not need to look neat and tidy.

     

     

    If you would prefer to use a glue then thermal double-sided adhesive tape or heat-resistant glue may be worth considering in order to help to avoid the adhesive becoming unbonded as temperature rises.

    0
    Comment actions Permalink

Please sign in to leave a comment.