What type of glue for placing IR filer to D 415 camera
Hi,
I want to glue your purchased IR filter to the camera module D415 C. The glue use so far is not great. Can you recommend a glue?
Kind regards, Karin
-
Hi Karin Dijkstra A RealSense user once used rubber bands instead of glue to hold an external ND filter to the front of the camera, so that solution may be worth considering if the camera does not need to look neat and tidy.

If you would prefer to use a glue then thermal double-sided adhesive tape or heat-resistant glue may be worth considering in order to help to avoid the adhesive becoming unbonded as temperature rises.
Please sign in to leave a comment.
Comments
1 comment