RealSense Support

Realsense D457 needs any additional equipment to work?

Comments

1 comment

  • MartyG

    By default the D457 camera model operates as a MIPI camera that requires a compatible deserializer product to be purchased separately (a popular choice is one from a company called Leopard Imaging) and also a special software driver.  The camera will not function on a GMSL/FAKRA cable connection without these.

     

    However, if you purchase a D457-compatible computer system from the company Connect Tech then it is not necessary to purchase the deserializer as the necessary technology is included in their product.  They also provide a driver.

     

    Further Information about the subjects mentioned above can be found at the following links.  

    https://github.com/IntelRealSense/librealsense/issues/10984#issuecomment-1363683498

    https://connecttech.com/connect-tech-offers-built-in-support-on-the-newly-announced-intel-gmsl-realsense-depth-camera-d457/

     

    If a physical switch in the D457's casing is moved sidewards though then the camera can use a USB cable connection like the other cameras in the RealSense 400 Series range and be detected as the D455 model.  When switched into USB mode, a deserializer board and the special driver are not required and the camera works when simply inserted into a USB port.

     

    If you have no plans to use the MIPI functionality then a D456 camera would be an appropriate alternative choice, as it behaves as a D455 and has the same protection against water and dust as D457.  

    0
    Comment actions Permalink

Please sign in to leave a comment.