Release Date of Intel Realsense D455if
Hello,
when is the release date for D455if (assuming that it is in development, since 455f performs better than 435f in manner of range errors %2 in 2m vs %2 in 4m)?
-
Hi Eguenay There is not a need for a D455if model (the i refers to a RealSense camera equipped with an IMU component). This is because the basic D455 model was launched with an IMU in it. So if D455f is purchased then it is like a D435if as it has an IMU (i) and the filter (f).
Please sign in to leave a comment.

Comments
2 comments