Port 2.1a port 3.0 configuration on realsense d457
Hi, I use the camara D457 when I connect the camera to the computer to port 3.0 with a cable 3.0 the realsense viewer detect the port like 2.1 how i can do to for detect usb 3.0?
-
Hi Mibarrar1902 When the D457 is used in USB mode, it may be constantly detected as USB 2.1 instead of USB 3.2 if the micro-sized end of the USB cable is inserted into the base of the camera in a particular direction of the two insertion directions available.
Is the D457 detected as 3.2 if you unplug the micro-sized connector from the base of the camera, turn it around the opposite way and re-insert it, please?
Please sign in to leave a comment.
Comments
2 comments