View my account

Port 2.1a port 3.0 configuration on realsense d457

Comments

2 comments

  • MartyG

    Hi Mibarrar1902  When the D457 is used in USB mode, it may be constantly detected as USB 2.1 instead of USB 3.2 if the micro-sized end of the USB cable is inserted into the base of the camera in a particular direction of the two insertion directions available. 

     

    Is the D457 detected as 3.2 if you unplug the micro-sized connector from the base of the camera, turn it around the opposite way and re-insert it, please?

    0
    Comment actions Permalink
  • Mibarrar1902

    Thank you very much now it works

    0
    Comment actions Permalink

Please sign in to leave a comment.