View my account

D456 vs D455f

Comments

1 comment

  • MartyG

    Hi Yenyen841009  

     

    The D457 model can operate in USB mode by moving a switch in the casing.  However, if you do not need a GMSL/FAKRA connection then D456 has the same water-resistant casing as the D457.

     

    The light-blocking filter on D455f can provide an improved depth image by being able to better deal with light reflections and negate disruptive 'repetitive patterns' (repeating horizontal or vertical patterns in the scene such as tiles on the ceiling or floor).  So if you do not require waterproofing then D455f is likely to be the appropriate choice for you. 

    0
    Comment actions Permalink

Please sign in to leave a comment.