RealSense Support

use D455 to take photos

Comments

3 comments

  • MartyG

    Hi Lizhirong597  In infrared mode the possibilities for adjusting the image are limited.  I would suggest using the exposure and gain defaults of 33000 exposure and 16 gain, and set laser power to its maximum of 360 in order to brighten the image.

    0
    Comment actions Permalink
  • Lizhirong597

    Thank you for your reply! I feel like I can't always focus well when I'm shooting, even though I've moved the camera from front to back, causing the image to be very blurry. Can you tell me how to determine the appropriate shooting distance? Are there any other parameters I can adjust? Do I need to turn on automatic exposure?

    The following is the matlab code for adjusting the parameters.

    As well as two photos of the left and right cameras, you can see that the ‘DEPTH CAMERA D455’ is relatively blurry.

    function adjust_depth_sensor_parameters(new_exposure, new_gain,enable_auto_exposure,new_laser_power)
        % 清除命令窗口,关闭所有图形窗口
        clc;
        close all;

        % 创建RealSense管道
        pipe = realsense.pipeline();
        
        % 启动管道,使用默认配置
        profile = pipe.start();
        
        % 获取设备对象
        dev = profile.get_device();
        
        % 获取第一个深度传感器
        depth_sensor = dev.first('depth_sensor');
        
        % 修改并显示新的曝光值
        try
            depth_sensor.set_option(realsense.option.exposure, new_exposure);
            current_exposure = depth_sensor.get_option(realsense.option.exposure);
            disp(['New exposure set to: ', num2str(current_exposure)]);
        catch ME
            disp(['Failed to set new exposure value: ', ME.message]);
        end

        % 修改并显示新的增益值
        try
            depth_sensor.set_option(realsense.option.gain, new_gain);
            current_gain = depth_sensor.get_option(realsense.option.gain);
            disp(['New gain set to: ', num2str(current_gain)]);
        catch ME
            disp(['Failed to set new gain value: ', ME.message]);
        end
        
        % 自动曝光
        try
            depth_sensor.set_option(realsense.option.enable_auto_exposure, enable_auto_exposure); % 1启用 0不启用
            disp(['Auto exposure set to:',num2str(enable_auto_exposure)]);
        catch ME
            disp(['Failed to enable auto exposure: ', ME.message]);
        end
        %激光功率
        try
            depth_sensor.set_option(realsense.option.laser_power, new_laser_power);
            % 获取并显示当前的激光功率
            current_laser_power = depth_sensor.get_option(realsense.option.laser_power);
            disp(['New laser power set to: ', num2str(current_laser_power)]);
        catch ME
            disp(['Failed to set new laser power: ', ME.message]);
        end
        
        % 停止管道
        pipe.stop();
    end

    0
    Comment actions Permalink
  • MartyG

    I would expect the quality of the infrared image to be relatively consistent no matter how near or distant the camera is.

     

    If you are experiencing blurring then if you are on a USB 3.2 connection you could consider defining custom stream configurations with cfg statements and using 848x480 resolution and 60 FPS (instead of the default 30 FPS).  As Infrared 2 (right infrared) is not available on a USB 2.1 camera connection, I assume that your connection is USB 3.2. 

    0
    Comment actions Permalink

Please sign in to leave a comment.