RealSense Support

No Frames received on D435 with USB2.1

Comments

1 comment

  • MartyG

    Hi Ron Vis  I can recall only two past occurrences of this issue with frames not being received unless firmware logging is enabled, including the case that you linked to.  This high rarity makes it likely that it is a glitch specific to a very small number of PCs rather than a more widespread bug, and there is therefore no known workaround.  The rarity also makes it unlikely that the issue will be experienced on different computers.

     

    I would suspect that the retrieval of firmware logs may be able to be repeated in code using the RS2_CAMERA_INFO_DEBUG_OP_CODE instruction.

    https://unanancyowen.github.io/librealsense2_apireference/rs__sensor_8h.html#aa607d93c1bac40af3ec1c9b0345f59af

     

    A C++ tutorial at the link below provides an example of using this instruction for printing the firmware log values.

    https://peteohanlon.wordpress.com/2018/03/09/662/

    0
    Comment actions Permalink

Please sign in to leave a comment.