RealSense Support

Ideal range of camera

Comments

2 comments

  • MartyG

    Hi Sohwa427  Ideal range applies only to the depth sensing.  It is the range in which you will get the optimal depth accuracy.  The RGB and infrared streams can see much further as they do not have the distance limitations of the depth stream. 

     

    Yes, D405 can depth-sense further than 0.5 m.  As distance from the camera increases, depth error increases.  The image below is of a window approximately 2 m from a D405.

     

    0
    Comment actions Permalink
  • Sohwa427

    Thanks MartyG

    You always give me a great responses!

    I can understand the specification better from your answers, and also thanks for the great example.

    0
    Comment actions Permalink

Please sign in to leave a comment.