RealSense Support

D455 Sometimes depth data is not updated.

Comments

14 comments

  • MartyG

    Hi Kawasyuuqq  Do you experience similar problems if you test the Python keypress capture script at the link below, please?

    https://github.com/IntelRealSense/librealsense/issues/8388#issuecomment-782395443

    0
    Comment actions Permalink
  • Kawasyuuqq

    Hi MartyG, thank you for your response.

    When I started this software, after a few seconds after startup, the following was repeated in a cycle of about 1 second.
    1. the software will not be able to acquire depth data at all, as shown in the attached image.
    2. The range where normal depths are acquired gradually expands.
    The camera stayed in this state for a few minutes, but when I moved the object in the camera or moved my hand near the object, the depth camera suddenly returned to normal.
    It did not happen every time. (It happens about 20~30% of the time when I start the software).
    I trimmed only the depth data and posted it.
    I took a picture of a stopped object.

    0
    Comment actions Permalink
  • MartyG

    If the image freezes or severely deteriorates in quality but the recovers after the camera is moved or covered over with the hand then this can be symptomatic of the camera having been faced directly towards a strong light source such as the sun.  Doing so can cause the sensors to become saturated with light.  Covering the camera lenses for a moment or turning the camera away from the light can enable auto-exposure to perform a correction.

    0
    Comment actions Permalink
  • Kawasyuuqq

    Sorry for the delay. And thanks for the reply.

    I ran the program linked above again.

    If I run the program approximately 5-10 times and each time I press the S key several times, the depth data stops updating once.
    Once it stops, it does not move again no matter how many times the S key is pressed.
    However, the color data never stopped.

    I initially used a long camera cable, but changing to the supplied cable did not fix this phenomenon.
    I would like to use a longer cable if possible because of the distance between the PC and the camera.

    0
    Comment actions Permalink
  • MartyG

    You are very welcome.  It's no trouble at all.  :)

     

    If you need to use a longer USB cable then the cable should be a high quality one designed for handing data transfer.  If the length is 5 meters or over then it is also recommendable to select one with active repeater components inside it so that the signal is boosted as it travels along the cable distance.  A company called Newnex supply high quality RealSense-validated cables, and also fiber optic cabling for much longer RealSense connections.

    0
    Comment actions Permalink
  • Kawasyuuqq

    Thanks. I will consider using that.
    Another problem, as I mentioned in one of my previous posts, sometimes only the depth data is not updated, even when I run the capture script in the following link
    https://github.com/IntelRealSense/librealsense/issues/8388#issuecomment-782395443
    However, I have changed the following settings to see the depth data in detail.
    resolution_width = 1280 # pixels
    resolution_height = 720 # pixels
    frame_rate = 5 # fps

    Sometimes the depth data stopped updating when I pressed the S key, and sometimes the depth data stopped updating a few seconds after startup even if I did not do anything.
    It does not happen every time. 
    What do you think is the reason why only the depth data stops updating?

    0
    Comment actions Permalink
  • MartyG

    I do not think that initialize_rs being called more than once and looping, otherwise there would be an error if the pipeline was attempted to be started when it was already active.

     

    If depth stops working even when nothing is done then I would recommend looking at your keypress listener code.  If you comment out the keypress listener mechanism and the program works okay when it is left to run without key input then that would be evidence that the problem is in the keypress code.

    0
    Comment actions Permalink
  • Kawasyuuqq

    I commented out the keypress part and ran the script again.
    However, the problem reappeared.
    I ran the script again with the "Intel Real Sense Viewer" (v2.54.2) open.
    At that time, a red square appeared on the right side of the screen, as shown in the image.

     

    When I clicked on it, the first one said "Severity: Error Description: Right MIPI error".
    The second one said "Severity: Error Description: Depth stream start failure.
    The third message was the same as the first one.
    Sometimes said "Severity: Error Description: REC error".

    0
    Comment actions Permalink
  • MartyG

    Which firmware driver version is installed in your camera, please?  You can find this information by clicking on the Info button near the top of the RealSense Viewer's options side-panel.

     

    If your currently installed Viewer version is 2.54.2 then the firmware driver version that should be installed in your camera is 5.15.1.0.  Using an older or newer firmware with 2.54.2 could result in errors occurring.

    0
    Comment actions Permalink
  • Kawasyuuqq

    I checked the version and it was 5.15.1.0.
    Both viewer and firmware versions were raised.
    Viewer: v2.55.1
    Firmware: 5.16.0.1


    However, the problem still occurs.
    I have also done some verifications. If you think this is not related to the matter of depth data not being updated, please ignore it.

    When I run "rs-multicam.exe", sometimes the depth data is messed up. (Same as 2 months ago).
    Also, the white line of the gyro is pointing in different directions, even though the camera is fixed to face downwards.
    When I run "rs-motion.exe", the camera turns around the red axis like a swing.
    This problem does not seem to occur when I open the Motion Module in the Viewer.
    I bought another camera of the same type, so I did the same verification. The result was the same as the first camera.

    0
    Comment actions Permalink
  • MartyG

    Thank you for the additional information.  What is the computer / computing device that you are running the Viewer and RealSense programs on, please?

    0
    Comment actions Permalink
  • Kawasyuuqq

     

    OS Windows10Pro
    OS Version 22H2
    OS build 19045.4412
    system type 64bit operating system,x64-based processor
    processor Intel(R) Core(TM) i7-9700K CPU @ 3.60GHz 3.60 GHz
    RAM 16GB

    Please let me know if there is any other information needed, as I am not sure what is needed.

    0
    Comment actions Permalink
  • MartyG

    Thank you, your computer's specification looks fine.

     

    Is there any improvement if you reset the camera hardware to its default factory-new calibration using the instructions at the link below?

    https://github.com/IntelRealSense/librealsense/issues/10182#issuecomment-1019854487

    0
    Comment actions Permalink

Please sign in to leave a comment.