RealSense Support

D405 surface depth resolution

Comments

1 comment

  • MartyG

    Hi Nh438999  The RealSense D405 camera model is not equipped with an infrared projector component.  On models that have this projector, the camera can cast a semi-random pattern of invisible dots onto surfaces in the real-world scene to aid the camera's depth analysis.  Without this pattern, the camera has greater difficulty analyzing plain surfaces that have little texture or no texture.  The plastic of a computer mouse would have such a surface.

     

    In the absence of a dot pattern, RealSense 400 Series cameras can make use of the ambient light in a scene to aid depth analysis.  So increasing the level of illumination in the scene (perhaps by adding a lamp) may help to improve the depth image.

     

    If the color of the mouse is dark gray or black then this could also negatively affect the depth image.  This is because it is a general physics principle (not specific to RealSense) that dark gray or black absorbs light and so makes it more difficult for depth cameras to read depth information from such surfaces.  The darker the color shade, the more light that is absorbed and so the less depth detail that the camera can obtain.  Again, casting a strong light source onto such surfaces can help to bring out depth detail.

     

    I would also recommend trying the Medium Density Visual Preset instead of the 'Default' one that you have set in the image above, as Medium Density provides a good balance between accuracy and the amount of detail on the depth image.

    0
    Comment actions Permalink

Please sign in to leave a comment.