RealSense Support

D405 "HW not ready" error implications

Comments

4 comments

  • MartyG

    Hi Toni Divic  You are correct, the auto_exposure_limit error is caused by using firmware version 5.15.1.0, which is designed for use with RealSense SDK version 2.54.2.  If you go to the firmware Releases page at the link below and find the ROS2 wrapper that you are using, the Recommended Firmware section of the information listing will show which firmware is recommended for that particular wrapper version.

    https://github.com/IntelRealSense/realsense-ros/releases

    0
    Comment actions Permalink
  • Toni Divic

    Ok that helps a bit, but doesn't answer the core part of my question: After the error occurs twice in a single launch, the camera eventually comes up. Does that mean the HW was eventually ready and the error has now gone away, or does the system just ignore the error and the auto_exposure_limit is never properly set?

    0
    Comment actions Permalink
  • MartyG

    Sometimes you can force your way past an error pop-up box by repeatedly clicking the OK button and then the camera may be detected and function normally afterwards.  The ideal situation is to avoid the pop-up completely though by having the recommended firmware for a particular SDK version installed.

    0
    Comment actions Permalink
  • Toni Divic

    Sounds good, thank you!

    0
    Comment actions Permalink

Please sign in to leave a comment.