Toni Divic
- Total activity 35
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 8
Activity overview
Latest activity by Toni Divic-
Toni Divic commented,
Great, thanks so much for the help. I'll try your suggestions and see where it leads
-
Toni Divic commented,
Couple of follow-up questions though based on what you said: Is there a Medium Accuracy preset? I'm not seeing that, I see High Accuracy or Medium Density (among a few others) We're launching th...
-
Toni Divic created a post,
Modify HighAccuracy preset to allow lower confidence points
In our application, we've been using the HighAccuracy json preset with pretty good success. However, we're noticing there are some situations where we have fewer points than we'd like, so we're cur...
-
Toni Divic commented,
(In terms of creating cases)
-
Toni Divic commented,
Ok. Are there recommendations for how cameras should be housed in outdoor storage environments to reduce impact of (temporary) degradation?
-
Toni Divic commented,
Interesting, glad to hear it's happened before. Is there a post for that case, and did they ever identify what the cause was?
-
Toni Divic created a post,
D405 performance lost then magically restored with no change
Hunting a bit of a weird failure mode and would appreciate some input! I've got 2 D405 cameras that we verified as working great in our lab environment. These then went to their working environment...
-
Toni Divic commented,
Found my issue: I had changed the resolution of depth_module and rgb_camera to 848x480, but I forgot that I was also setting the depth_module.auto_exposure_roi manually and had left the right value...
-
Toni Divic commented,
It is a Jetson running Ubuntu 20.04.6. I did just try launch directly with rs_launch.py and it works when I pass in 848x480 via command line. I'll take a look to see if somehow our launch file (whi...
-
Toni Divic commented,
Got it, when I look at the launch log for the versions it says I'm running with the following RealSense ROS v4.51.1Built with LibRealSense v2.51.1Running with LibRealSense v2.51.1 However when I ...