RealSense D435 Distortion Model
Hi,
I am wondering what distortion model the Intel RealSense D435 is? I can't find information about it, other than general models used by the depth cameras listed (but not specified to each camera model). These are found in the following two links:
https://dev.intelrealsense.com/docs/projection-in-intel-realsense-sdk-20#point-cloud
https://dev.intelrealsense.com/docs/projection-texture-mapping-and-occlusion-with-intel-realsense-depth-cameras
I have extracted the intrinsic parameters from my camera. I used CustomRW for resetting to factory gold settings, and extracting the parameters, which are:
FocalLengthColor: 1379.333496, 1378.66125
PrincipalPointColor: 973.144470, 535.20050
distortionCoefficients = [ 0.0 0.0 0.0 0.0 0.0 ]
Given the fact that the distortion coefficients are set to 0, I want to set up the assumption that we can use the Idealized Pinhole Model, but I want clarification on this before saying so, as it is for my bachelor thesis (where I want the information to be correct). Furthermore, if the idealized model is acceptable, how may I argue for it being so? Is it due to the factory calibration, or because of physical properties?
Help would be greatly appreciated.
Best regards,
Thomas.
-
Hi Thomal2002 You can list the intrinsics for a specific RealSense camera (including the distortion model used by each stream type) using the calibration information mode of the RealSense SDK's rs-enumerate-devices tool. It can be launched in calibration information mode with the command below:
rs-enumerate-devices -c

I do not have advice that I can offer about the Idealized Pinhole Model, unfortunately.
Please sign in to leave a comment.
Comments
2 comments