Matlab Developer Package
According to the documentation (https://github.com/IntelRealSense/librealsense/tree/development/wrappers/matlab), the Windows Installer for the RealSense SDK 2.0 should provide the option to install the Matlab Developer Package. However, mine doesn't seem to have that option (I am installing SDK 2.0 v2.54.2). Do you know where I can access it from?

-
Hi Tpike The MATLAB developer package is included in the 2.54.1 installer but not in 2.54.2.
https://github.com/IntelRealSense/librealsense/releases/tag/v2.54.1
You should be able to obtain the package by installing the 2.54.1 SDK using its installer program. Afterwards, run the 2.54.2 installer program again - you should not need to download it again as it will still be in your Downloads folder. Then 2.54.2 will be installed but the MATLAB package from 2.54.1 will still be there. This is because if a package is missing from the installer, earlier versions of that package that are on your computer are not removed.
Please sign in to leave a comment.
Comments
2 comments