RealSense Support

Unable to Access realsense D457 Device After Firmware Update Failure

Comments

5 comments

  • MartyG

    Hi Melebele3073  The intel-realsense-dfu.exe DFU firmware update tool was the original firmware update tool for the RealSense 400 Series cameras dating back to late 2017, but it has long since been superseded by rs-fw-update and the firmware updater mechanism in the RealSense Viewer tool.  intel-realsense-dfu.exe is designed only for the D415 and D435 camera models.

     

    In the Windows environment, the rs-fw-update tool must be run from the Windows Command Prompt text interface rather than double-leftclicking on the rs-fw-update.exe file in the SDK Tools folder, as advised at the link below.

    https://github.com/IntelRealSense/librealsense/issues/8500#issuecomment-791540583

     

    Version 2.54.2 of the RealSense SDK added support for updating D457 firmware with rs-fw-update over a MIPI connection instead of USB.

    https://github.com/IntelRealSense/librealsense/releases/tag/v2.54.2

     

    In the RealSense Viewer tool, if the camera is listed in the options side-panel then you can update the firmware by going to the More option near the top of the side-panel and selecting Update Firmware from its drop-down menu.

    0
    Comment actions Permalink
  • Melebele3073

    At the moment, I don't have an MIPI connector available, so testing is not feasible right now. If I obtain an MIPI connector in the future, I will certainly give it a try.

    However, judging from the device status reported by lsusb, I don't think I can be particularly optimistic about the outcome.

     

    And it seems like there's no separate MIPI port on the device. Can you tell me which cable to use and where to plug it in?

     

    Regarding the RealSense Viewer, as I mentioned earlier, it is not recognizing the device, and the camera is not appearing in the connected device list. Therefore, updating through the RealSense Viewer is currently not possible.

    I've added a few more screenshots to my initial post. Please take a look at them for reference in finding a solution.

    0
    Comment actions Permalink
  • MartyG

    Thanks very much for the additional screenshots, which were helpful.

     

    The connector for plugging a GMSL / FAKRA cable into the camera for use on a MIPI connection is on the side of the camera underneath a large removable side-cap on the camera casing.

     

    On a USB connection the camera should be detected as D455 if the firmware is working correctly.

     

    As mentioned in the similar case that you linked to at the beginning of this discussion, a camera with the Invalid SKU error may be recoverable if the casing is opened and a cable joining two circuit boards together is disconnected and a firmware update then attempted.  Doing so would likely invalidate the sales warranty of the camera though.

    https://support.intelrealsense.com/hc/en-us/community/posts/15226169805971/comments/15355576689939

     

    As the D457 model has been available for almost exactly a year at the time of writing this, your camera should still be within the 1 year sales warranty period after purchase, 

    0
    Comment actions Permalink
  • Melebele3073

    Thank you for your response.

    I'm concerned about voiding the camera's warranty, but would this method definitely result in successful recovery? I'd like to confirm the exact procedure. To attempt recovery this way, should I connect the camera to a Raspberry Pi or a similar device using an MIPI cable, install the RealSense Viewer, and run it? If this program can successfully recognize the device without any issues, and I proceed with the update through the RealSense Viewer, will the camera be restored without any problems? I'd also like to find a solution that doesn't void the warranty. I believe it hasn't been a year since the purchase, and I bought it through a distributor while residing overseas, with an official warranty sticker from the distributor. Is it possible to receive service in this case?

    0
    Comment actions Permalink
  • MartyG

    If you are not familiar with opening and handling electronic components then I would recommending enquiring first to the retailer that you purchased it from about an RMA return.

    0
    Comment actions Permalink

Please sign in to leave a comment.