D415 RGB Resolution
Hi, on the page of the D415 the RGB frame resolution is stated as 1920 x 1080.
When retrieving the picture using the SDK I always get an image of 1280 x 720. I'm probably doing something wrong. Does anyone have an idea?
Kind regards,
Joe
-
Hi Eskimos Nl+realsense The D415's default RGB resolution is 1280x720. If you are using the RealSense Viewer tool then you can choose 1920x1080 from the resolution selection drop-down in the RGB section of the Viewer's options side-panel.

If you are writing your own program then you can override the default and set your chosen resolution using a cfg stream configuration line. For example:
cfg.enable_stream(rs.stream.color, 1920, 1080, rs.format.rgb8, 30)
Please sign in to leave a comment.
Comments
2 comments